Mouser Press Room
Mouser Facebook Mouser Twitter Mouser RSS Feed Mouser YouTube Channel Mouser Google+ Mouser LinkedIn Mouser Subscription Center Mouser Blog
Mouser Press Room
New Product Announcement

Takeoff Designing with the TI MSP-EXP432P401R 32 bit LaunchPad Evaluation Kit Now at Mouser

April 1, 2015 - Mouser Electronics, Inc. is now stocking the MSP-EXP432P401R LaunchPad Evaluation Kit from Texas Instruments (TI). This new TI LaunchPad is an easy-to-use rapid-prototyping kit for TI's new MSP432P401R microcontrollers featuring 256KBytes of Flash and 64K of SRAM. The new TI MSP432™ microcontroller family is based on a low power ARM® Cortex‑M4F and draws as little as 800nA in low power mode, with a run current of 95µA/MHz. The MSP432P401R 32‑bit microcontroller supports speeds up to 48MHz and has integrated peripherals for communication, ADC, timers, and AES encryption.

The TI MSP-EXP432P401R LaunchPad Evaluation Kit, available from Mouser Electronics, provides a platform for evaluating the new TI MSP432P401R microcontroller. The MSP432 MCU's ARM Cortex‑M4F core is a powerful 32‑bit CPU with a floating point unit and memory protection management. The microcontroller includes two 16‑bit timers, four 32‑bit timers, and a 24‑channel 14‑bit analog to digital converter (ADC) that converts at 1MSPS. The microcontroller also boasts four high-drive I/O pins that can support up to 20mA. The microcontroller can draw as little as 90µA at a clock speed of 128kHz. Capacitive touch capability is supported as well as digital glitch filtering on some I/O pins. The onboard DSP instructions and floating point unit enable a wide variety of low power high performance processing, including signal conditioning and sensor fusion.

The MSP-EXP432P401R LaunchPad Kit has a simple user interface through two on-board buttons and two multicolor LEDs. Additional features include an onboard XDS110‑ET open source debugger with TI's EnergyTrace+™ Technology that enables developers to analyze power consumption in real time. To allow for rapid prototyping, the kit also features a 20-pin LaunchPad standard that leverages the BoosterPack ecosystem. TI's BoosterPacks enable technologies such as wireless connectivity, graphical displays, and environmental sensing.

The MSP432 MCU Platform supports individual program control over each of its eight RAM banks, allowing each bank to be turned on or off. This saves power by deactivating unused banks of memory.

The MSP-EXP432P401R LaunchPad Development Kit, now available through Mouser Electronics, includes the MSP-EXP432P401R evaluation board, a micro USB cable and a quick start guide. The evaluation kit, combined with the MSP432P401R microcontroller, gives designers the freedom to develop for a variety of low-power applications, ranging from smart meters, portable medical devices, the Internet of Things (IoT), industrial and remote sensors, home automation and energy harvesting.

To learn more about the MSP432 LaunchPad, visit:
http://www.mouser.com/new/Texas-Instruments/ti-msp-exp432p401r-kit/ .

To learn more about the MSP432 MCU, visit: http://www.mouser.com/ti-msp432-microcontrollers/ .

With its broad product line and unsurpassed customer service, Mouser caters to design engineers and buyers by delivering What's Next in advanced technologies. Mouser offers customers 20 global support locations and the latest, most technologically advanced components for their newest design projects. Mouser Electronics' website is updated daily and searches more than 10 million products to locate over 4 million orderable part numbers available for easy online purchase. Mouser.com also houses an industry-first interactive catalog, data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.

About Mouser Electronics
Mouser Electronics, a subsidiary of TTI, Inc., is part of Warren Buffett's Berkshire Hathaway family of companies. Mouser is an award-winning authorized semiconductor and electronic component distributor, focused on the rapid introduction of new products and technologies to electronic design engineers and buyers. Mouser.com features more than 4 million products online from more than 500 manufacturers. Mouser publishes multiple catalogs per year providing designers with up-to-date data on the components now available for the next generation of electronic devices. Mouser ships globally to over 400,000 customers in 170 countries from its 492,000 sq. ft. state-of-the-art facility south of Dallas, Texas. For more information, visit www.mouser.com.

Trademarks
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.



Further information, contact:
Kevin Hess, Mouser Electronics
Vice President Technical Marketing
(817) 804-3833
Kevin.Hess@mouser.com
For press inquiries, contact:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
(817) 804-7764
Kelly.DeGarmo@mouser.com
Back to Press Room