Editor’s note: In April, 2017, Mouser hosted the webinar, “ Bluetooth 5: Reinventing Connectivity and Advancing Industrial IoT.” This is one of many great questions (and answers) that came from the webinar.
Viewer Question: Do you know if it will be possible to have long range and mesh (when SIG releases) simultaneously with Bluetooth 5?
Answer: Thanks for your question…it's a good one! The general answer is "yes but."
As you know, range is determined by many factors, and mesh networking works to minimize their effects so that a network can be expanded in area and number of connected devices by reducing the distance over which any connected node must communicate. That is, nodes are connected together rather than as in a star topology to go back to a hub or gateway. This effectively reduces the need to have “long-range” capabilities.
For example, let’s say a Bluetooth device transmitting at its highest permissible output power covers (in this instance) 400ft. To have some margin, you wouldn’t place devices that far apart because you want the Bluetooth-enabled sensors to use as little DC power as possible. The mesh makes this possible.
For more information about Bluetooth, visit the Mouser RF Wireless site.
Barry Manz is president of Manz Communications, Inc., a technical media relations agency he founded in 1987. He has since worked with more than 100 companies in the RF and microwave, defense, test and measurement, semiconductor, embedded systems, lightwave, and other markets. Barry writes articles for print and online trade publications, as well as white papers, application notes, symposium papers, technical references guides, and Web content. He is also a contributing editor for the Journal of Electronic Defense, editor of Military Microwave Digest, co-founder of MilCOTS Digest magazine, and was editor in chief of Microwaves & RF magazine.